EMO 2023
Product highlights
CNC
Next-generation CNC technology
Have a glimpse into the future of CNC technology, and discover the future FS500i-A series, presented in Europe for the first time. Optimised for performance, the new CNC series will offer a number of important innovations.
DISCOVER MOREROBOMACHINE
Driving innovation: The power of a fully automated production cell
The machining of a complex EV (electric vehicle) part in four and five axes will be simulated by a complete production cell, consisting of 2 ROBODRILL α-DiB Plus series machining centres, a FANUC M-20iD/25 robot on a linear rail for machine tending, an AGV (automated guided vehicle) for exchanging raw and finished part pallets, a CMM (co-ordinate measuring machine) for part measurement, and sensor and connectivity technology to provide feedback from the CMM to the ROBOMACHINEs, for example. Two ROBOCUT α-CiC wire EDM machines will also be part of the system.
Unbeatable versatility and flexibility
The new addition to the Advanced Plus ROBODRILL series will be presented in Europe for the first time. Designed to cover a wider range of machining tasks involving large workpieces, such as EV parts, FANUC ROBODRILL α-D28LiB5ADV Plus Y500 offers maximum flexibility through a Y-axis stroke of 500 mm and an increased table size. It features an increased tool capacity of 28 tools.
DISCOVER MOREUnmatched wire EDM versatility
Making its world premiere at EMO will be the FANUC ROBOCUT α-C800iC wire EDM, an 800 mm X-axis stroke machine that completes the ROBOCUT α-CiC family. At the show, this large-format machine is set to simulate the wire cutting of a complex aerospace turbine part.
DISCOVER MOREROBOTS
The new generation of the M-710 robot series
The successor to the M-710iC offers a higher payload and speed, as well as more wrist moment and inertia capabilities. Furthermore, a curved arm supports its use in applications involving tighter spaces, such as removing parts from a container. The M-710iD is set to perform a logistics application at EMO, which is just one of many possibilities for this versatile robot.
DISCOVER MOREThe strongest get even stronger
FANUC has been offering the most powerful collaborative robots on the market for several years. Meet the CRX-25iA collaborative robot with a 30 kg payload option and the CR-35iB collaborative robot with a heavy-duty 50 kg option at the FANUC booth.
DISCOVER MOREPowerful solution for demanding intelligent applications
The FANUC iPC Box provides a reliable industrial solution for advanced robot applications that require high computational performance. It is equipped with multiple Gigabit Ethernet ports and a powerful CPU for quick acquisition and processing of image data by iRVision software. Seamless integration with FANUC R-30iB Plus controller allows for ease of use, setup, commissioning and maintenance of your robot system.
DISCOVER MOREIoT
Data analysis on premise
FIELD system Basic Package is an on-premise platform (no Internet connection required) that allows manufacturers to collect, analyse and utilise data from connected machines and devices, offering compatibility with FANUC products up to 20 years old and extending its support to third-party products.
DISCOVER MORESERVICE
Real-time support from a distance
With the help of FAR (FANUC Assisted Reality), FANUC experienced service staff can see what the customer sees and quickly get an overview on-site, to facilitates the repair or diagnosis of FANUC products, enhancing operational efficiency.
DISCOVER MORE